Torque_slope

Index.Sub 6087.0H
Data Type Unsigned32
Access Read/Write
PDO Mappable RX_PDO (1)
Unit ‰ Nominal_Current /sec

Range

0 to 2147483647
Default Value 10000
Store Supported Yes
Description

This object defines the slope for Profile Torque mode (tq) and Cyclic Synchronous Torque (cst) modes. The value is considered proportional to Nominal_Current (Motor rated current). The value is defined as units of thousandths of the torque per second. 

Notes

(1) available with firmware V03r03 or superior.

  • This object is available only with firmware version V03r03 or superior.